Search FAQs
Does the ATV340 keypad (VW3A1113) have its own mounting kit?
Issue:
What is the part number of the mounting kit for the ATV340 keypad (VW3A1113)?
Product Line:
Altivar Drives
Environment:
Open style drive
Cause:
Mounting kit for VW3A1113
Resolution:
Frame sizes 1-3 have the ability to mount the VW3A1113 directly on the front of the drive.
VW3A1114 is the part number for the keypad mounting kit..
![Keypad mounting kit Keypad mounting kit](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000008zrvoQAA&oid=00DA0000000abSm)
The Altivar 340 drive can also use the Graphic Display Terminal VW3A1111 (also used on the Altivar Process Drives), which can be connected to the drive using the Remote mount kit (VW3A1112) and a Modbus cable.
Frame sizes 4 and 5 allow mounting of the VW3A1111 display directly on the front of the drive.
NOTE: The drive does not come with either of these displays. They must be ordered separately.
What is the part number of the mounting kit for the ATV340 keypad (VW3A1113)?
Product Line:
Altivar Drives
Environment:
Open style drive
Cause:
Mounting kit for VW3A1113
Resolution:
Frame sizes 1-3 have the ability to mount the VW3A1113 directly on the front of the drive.
VW3A1114 is the part number for the keypad mounting kit..
The Altivar 340 drive can also use the Graphic Display Terminal VW3A1111 (also used on the Altivar Process Drives), which can be connected to the drive using the Remote mount kit (VW3A1112) and a Modbus cable.
Frame sizes 4 and 5 allow mounting of the VW3A1111 display directly on the front of the drive.
NOTE: The drive does not come with either of these displays. They must be ordered separately.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Product:
Explore more
Range:
Product: