This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
- The following points should be taken into account:
- Series wiring is only possible using sensors with wide voltage limits.
U sensor =U (supply) / n sensors
U sensor and U supply must remain within the sensor’s voltage limits.
- If only one sensor in the circuit is in the open state, it will be supplied at a voltage almost equal to the supply voltage.
- When in the closed state, a small voltage drop is present across each sensor. The resultant loss of voltage at the load will be the sum of the individual voltage drops and therefore, the load voltage should be selected accordingly.
Released for: Schneider Electric Egypt and North East Africa