{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to change Run command assignment to the Logic input different than DI1 of On frequency inverter Altivar Process ATV600, ATV900
When Altivar process is controlled via terminals and using 2-wire control it is always digital input 1 associated with the run forward (FWD) command. It is not possible to re-assign the run FWD command to other digital inputs.
Only run reverse is optional and can be assigned to any input.
Note that in 3-wire control the DI1 is assigned to stop and DI2 to run FWD. Not possible to change them.
See picture.
Although digital input 1 has a fixed assignment (run FWD in 2-wire control), it can also be assigned (multi-assignment) to an additional function.
E.g. DI1 = run FWD and preset speed 2

Schneider Electric Egypt and North East Africa

Attachment(s)
ATVp_terminal control.jpg [125.78 KB]