Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
What are inputs JerkRatio1-2-3-4 of MC_MoveVelocity_PTO ?
In Ecostruxure Machine Expert, the function block MC_Movelocity_PTO has 4 JerkRatio inputs.
-

JerkRatio1-4 are used to change the shape of the S-curve.

-
 
  • JerkRatio1: Percentage of acceleration from standstill used to create the S-curve profile
  • JerkRatio2: Percentage of acceleration to constant velocity used to create the S-curve profile
  • JerkRatio3: Percentage of deceleration from constant velocity used to create the S-curve profile
  • JerkRatio4: Percentage of deceleration to standstill used to create the S-curve profile

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: