{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can I mount the VW3A1101 keypad further than 30 feet away from an Altivar Drives?
Issue:
Customer needs to mount the VW3A1101 keypad further than the recommended 30 feet away from the drive.

Product line:
VW3A1101 keypad and all drives it is used with.

Environment:
All models and serial numbers

Cause:
Non-standard installation.  The maximum recommended distance using our supplied cables is 30 feet.

Resolution:
Please see attached drawing. It will be necessary to add in a splitter, coupler, and external 10VDC power supply capable of 100ma of current or greater.  These are generic parts that are widely available.



Schneider Electric Egypt and North East Africa

Attachment(s)
Extended keypad.pdf [126.55 KB]