Search FAQs
Why doesn't SoMove Software show all assigned inputs under the Operate Tab, Input/Output terminals?
Issue:
Why doesn't SoMove Software show all assigned inputs under the Operate Tab, Input/Output terminals?
Product Line:
Altivar Machines, SoMove Software
Environment:
All models and serial numbers
Cause:
Programming
Resolution:
Per Level 3 - There is a limitation on SoMove, we see only LI1 and LI2 logic input, no LI3 to LI6.
The limitation is to avoid SoMove Modbus overload which can cause SoMove untimely disconnection.
Why doesn't SoMove Software show all assigned inputs under the Operate Tab, Input/Output terminals?
Product Line:
Altivar Machines, SoMove Software
Environment:
All models and serial numbers
Cause:
Programming
Resolution:
Per Level 3 - There is a limitation on SoMove, we see only LI1 and LI2 logic input, no LI3 to LI6.
The limitation is to avoid SoMove Modbus overload which can cause SoMove untimely disconnection.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: