{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What to do if a message with ID 0x1450, 0x1451, 0x1452, 0x1453, 0x1454, 0x1455, 0x1456, 0x1457, 0x1458, or 0x1459 is displayed on the MicroLogic X screen.

These messages are generated by the Opening/Closing Monitoring function of the MicroLogic X control unit, to indicate that a predefined number of operations of the MCH gear motor or one of the voltage releases (MN, XF, MX1, or MX2) is reached.

Refer to the MicroLogic X User Guide:

Schneider Electric Egypt and North East Africa