Issue:
The touch screen calibration is still inaccurate even after using the Windows Control panel's Tablet PC Settings.
Product Line:
Magelis iPC, HMIBMU, HMIBMI
Resolution:
When calibrating the touchscreen of an HMIBMU or HMIBMI series, ensure not to use the Windows calibration tool. Instead, look for the PenMount Control Panel and use the calibration tool of that application. It provides the option for 25 points of calibration. By using 25 points, it gives the touchscreen a more accurate calibration.
The touch screen calibration is still inaccurate even after using the Windows Control panel's Tablet PC Settings.
Product Line:
Magelis iPC, HMIBMU, HMIBMI
Resolution:
When calibrating the touchscreen of an HMIBMU or HMIBMI series, ensure not to use the Windows calibration tool. Instead, look for the PenMount Control Panel and use the calibration tool of that application. It provides the option for 25 points of calibration. By using 25 points, it gives the touchscreen a more accurate calibration.
Released for:Schneider Electric Egypt and North East Africa