{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why I have some difficulties to connect to GateManager or LinkManager?
Issue
The GateManager version 8.3.19081 may have some compatibility issues with the browsers Internet Explorer 11 (IE11) and Mozilla Firefox.  These are experienced using the GateManager and LinkManager user interfaces.

Product Line
Offer impacted: Ecostruxure Secure Connect Advisor
Version of GateManager: 8.3.19081

Environment
Internet Explorer 11 (IE11) and Mozilla Firefox

Resolution
As a workaround, use another browser internet as Chrome

Schneider Electric Egypt and North East Africa