Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the power factor of induction motor at full load and no load?
The power factor of induction motors varies with load, typically from around 0.85 or 0.90 at full load to as low as about 0.20 at no-load.
At no load, an induction motor draws a large magnetizing current and a small active component to meet the no-load losses.
Therefore, the induction motor takes a high no-load current lagging the applied voltage by a large angle.
Hence the power factor of an induction motor on no load is low.
At no load, an induction motor draws a large magnetizing current and a small active component to meet the no-load losses.
Therefore, the induction motor takes a high no-load current lagging the applied voltage by a large angle.
Hence the power factor of an induction motor on no load is low.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: