Issue:
Number of RJ45 communication ports on a standard ATV630 drive
Product Line:
ATV630
Environment:
All serial numbers
Cause:
Customer wanted to know how many serial ports comes with the ATV630 drive.
Resolution:
The ATV630 has 2 built-in RJ45 communication ports as standard:
1 Ethernet Port (TCP only)
1 Modbus Serial Port
Number of RJ45 communication ports on a standard ATV630 drive
Product Line:
ATV630
Environment:
All serial numbers
Cause:
Customer wanted to know how many serial ports comes with the ATV630 drive.
Resolution:
The ATV630 has 2 built-in RJ45 communication ports as standard:
1 Ethernet Port (TCP only)
1 Modbus Serial Port
Released for:Schneider Electric Egypt and North East Africa