Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the difference between public and personal dashboards?
Dashboard is a new feature in Webstation 3.0. Dashboard is a “WebStation-only” feature which means you use WebStation to create, edit and display dashboards. There are no Dashboard editor or viewer in WorkStation, but the Dashboard and Widget objects are visible in WorkStation so it is possible to edit the object properties.
A dashboard can contain ready-to-use Widgets (diagrams and value presenters), custom Widgets (regular TGML Graphics objects) and Hyperlinks. Both historical and live values can be presented.
Room Last 7 Days 1200 AM cOO AM 6:00 AM 8:00 AM 10:00 AM 1200 PM 2:00 PM 4:00 PM PM too PM 10:00 PM perature Tu Last 24 Hours We 450 ppm 250 •c Last 7 Days over Previous 7 Days 24 •c 23.5 •c 23 •c 22.5 •c Temperature Previous 7 days I ast 7 days
Public Dashboards:
The Public Dashboard feature is available in WebStation 3.0 as a standard feature. Public dashboards are created and stored as any other object in the server tree.   Public dashboard can be created by any user that has access to the folder where the dashboards are located. Any user that has access to the folder can view the dashboard.
 
Personal Dashboards:
 Personal Dashboard is a licensed feature.  A Personal Dashboard is associated with the logged in user and is not stored together with the other application objects in the server tree. Part number of personal dashboards feature: SXWSWDASH00001.
For more information about dashboards, refer to Web Help:  How Dashboards Work.
Administration System tree A Favorite pages Public Dashboard Folder Name •e public Dashboard A Dashboards personal dashboard Personal Dashboard
 

Schneider Electric Egypt and North East Africa