Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How to reduce starting current in ATS22?
Starting current is set into soft starter based on type of application and load demand.
Current can be limited from ILt from 200 : 700 % In (Motor rated current) and default value is 350%.
Also,decreasing ACC (Acceleration time) to shorten the period of starting.

Note:

Proper fine-tuning of the starting current (ILt) setting has to be done during commissioning.
Normally the soft starter will work without any problem with current limit setting between 200% to 450% for different application starting torque requirement.
For example : for compressor application starting current received is approx. 3 to 4 times the rated motor current.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: