Search FAQs
PowerChute cannot be installed on 32-bit systems
Issue:
PowerChute cannot be installed on 32-bit systems.
Product Line:
PowerChute Business Edition
PowerChute Serial Shutdown
PowerChute Network Shutdown
Environment:
All supported OS
Cause:
Solution:
We no longer support 32-bit operating systems. To run PowerChute, upgrade the hardware to 64-bit.
PowerChute cannot be installed on 32-bit systems.
Product Line:
PowerChute Business Edition
PowerChute Serial Shutdown
PowerChute Network Shutdown
Environment:
All supported OS
Cause:
- PowerChute Serial Shutdown is a 64-bit-only application.
- PowerChute Business Edition v10.0 and above are 64-bit-only applications.
- PowerChute Network Shutdown v4.3 and above are 64-bit-only applications.
Solution:
We no longer support 32-bit operating systems. To run PowerChute, upgrade the hardware to 64-bit.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: