Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Magelis shows error "configuration file is not unicode"
Issue:
The Magelis HMI fails to boot properly and there is an application halt. The error on the dialog states the following:

Config problem:the configuration file is not unicode          
KAOScore:PortableProjectConfiguration.cpp:line 406


Product Line:
Magelis HMI programmed Vijeo Designer (any version)

Resolution:
This error is a result of a corrupt Vijeo Designer installation on the PC where the software is installed. To resolve this issue, please re-install Vijeo Designer and re-download to the HMI.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: