{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can PMEGPS0100 module be installed in M580 HSBY CPU rack.
Issue: Is it possible to install the PMEGPS0100 in M580 HSBY CPU Rack

Product line: PMEGPS0100

Environment : Control Expert V14 and Win 10 Professional build 10.1703.1

Resolution: The PMEGPS0100 is only be used in a remote Ethernet rack in a M580 HSBY system. The module can not be mounted in either HSBY CPU rack.
Like most DIO connections, the PLC Input data from a PMEGPS0100 module is not “bumpless” during a transfer from Secondary to the new Primary. The Ethernet/IP connections will be closed, and the module “Freshness” will drop to 0 during the transfer.

Schneider Electric Egypt and North East Africa