{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the pickup voltage for the RSB series relays?

Issue:
Voltage at which the coil will engage

Product line:
Relays and Timers

Environment:
RSB Zelio Plug in Relays

Cause:
Documents show drop out voltage not pick up voltage

Resolution:
The pickup up voltage is within 70% of the rated coil voltage.

So for example on RSB1A120ED with a 48VDC coil, the pick up voltage is 33.6VDC.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: