{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How can I connect Lighting circuits, on/off or dimming, to HRC controllers?

Lighting can be connected to HRC as shown in the following architecture, Consider the following:

  • Lighting on/off control, the use of 230VAC relay is a must.
  • For dimming, the current HRC only supports 0-10V. However, there may be cases of compatibility issues for certain dimming drivers, and therefore, it is recommended to test the compatibility in advance. In case of compatibility issues, adding a resistor (600Ω, 0.5W) in parallel with the dimming drive may solve the issue.

HRC connections

Schneider Electric Egypt and North East Africa