Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Video: How to create self-signed certificate in EBO Device Administrator?
Certificates are used to increase the security of the communication between Device Administrator and SmartX server. Certificates are used to establish a trust chain between Device Administrator and the SmartX servers. A trusted chain communication with HTTPS consists of two parts:
• An SSL root certificate installed in Windows on the computer that runs Device Administrator
• An SSL certificate on the SmartX server
Both Device Administrator and SmartX servers support self-signed certificates as well as CA certificates. Device Administrator allows you to create your own self-signed certificate, the following video shows steps to do that: 
 

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: