Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
How can I Search and Replace project variables used throughout a Control Expert project?

Issue
There are tools for searching and replacing variables either in the Data Editor or from a Variable search. Right clicking on Function blocks in logic after selecting them will allow a wildcard replace of variables on pins. These are cumbersome if a Global effort is underway where we want to search and replace all instances of a variable name whether in sections or the data editor. Is there an option other than these tools?

Product line
Control Expert, Unity Pro

Resolution

  1. Export the project to a ZEF file.
  2. Right click on the ZEF file and select  7-ZIP then Open archive. (or simply open it as an archive)
  3. Right click on the unitpro.xef file from the archive and select Edit (this should launch Notepad)
  4. Using Notepad's Edit - Search and Replace make the modifications.
  5. Save the unitpro.xef file. (this should update the unitpro.xef that is in the ZEF)
  6. Open the ZEF with Control Expert and you should see your changes.



If this FAQ did not solve your issue, you can chat with us at chat with us  or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
 
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
 

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: