Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What does 1 way, 2 way and intermediate light switching mean?
There are 3 basic types of switches that are used for domestic purposes:
  • 1 Way Switches: If a light switch is ‘1 way’ this means it is just an on/off switch. This is the simplest type of switch that you can get. The single switch controls a single light (or lighting circuit).
  • 2 Way Switches: A ‘2 way’ switch means there is another switch controlling the same light. These are often used on a stair case, large room with switches by each door.
  • Intermediate Switches: If you need to control the lights from three places, say you have 3 entrances to a large room and need a light switch next to each one, you will need an intermediate switch. The light(s) can be switched on and off from anyone of 3 places.

On the whole 2 or 3 gang switches will always be 2 way switches. If you are buying switches and don’t know exactly what you need, then it is often a good idea to get a 2 way switch anyway. This is because if you only need a 1 way switch, you can still use it by only connecting one of the terminals (L1 or L2) and common terminal. (If the switch doesn’t work the way you want it to, you can either turn the switch around or swap the L1 and L2 terminal).

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: