Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How many devices can control the Wiser for KNX device?
The Wiser for KNK (W4K) visualization is web based. So any device (connected to the same network as the W4K) having a web browser will be able to connect to the W4K IP address (default address: 192.168.0.10) and control the W4K. So many devices can login to the device and control it. Login credentials are illustrated in the attached instruction sheet (on the bottom left). At the same time, the User Manual of the W4K is provided in the attached link.
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Range:
Explore more
Range: