This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
The C60 (or iC60) offers are compliant with 60V DC per pole.
C120 / NG125 offers are compliant with 125V DC by pole
C60H-DC offer is compliant with 250V per pole.