Search FAQs
On an ATV21 or ATV212 how can the PID feedback be reversed?
Issue:
How do I reverse the PID feedback on an ATV21/212 drive?
Product Line:
Altivar 21, Altivar 212
Environment:
All
Cause:
Reversing the way the drive responds to feedback
Resolution:
If you want reverse the PID feedback, then you have to reverse the scaling of the analogue input (of the PID feedback) which has been chosen.
The scaling is set with the paramters : F201 up to F204 for VIA and F210 up to F213 for VIB.
Please, refer to the page F16-F17 of the user's manual.
For example, you have a 4-20mA sensor feedback on VIA and if you want reverse the scaling then set the parameter as follow :
F201=20% ; F202 = 60 HZ and F203 = 100% and F204 = 0 HZ.
How do I reverse the PID feedback on an ATV21/212 drive?
Product Line:
Altivar 21, Altivar 212
Environment:
All
Cause:
Reversing the way the drive responds to feedback
Resolution:
If you want reverse the PID feedback, then you have to reverse the scaling of the analogue input (of the PID feedback) which has been chosen.
The scaling is set with the paramters : F201 up to F204 for VIA and F210 up to F213 for VIB.
Please, refer to the page F16-F17 of the user's manual.
For example, you have a 4-20mA sensor feedback on VIA and if you want reverse the scaling then set the parameter as follow :
F201=20% ; F202 = 60 HZ and F203 = 100% and F204 = 0 HZ.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: