{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the ION9000 FTP file structure and permissions?
Issue
User needs to know the FTP file structure and permissions of ION9000.

Product Line
ION9000

Cause
FTP file structure and permissions of ION9000 are required.

Resolution
COMTRADE: COMTRADE files can be read from these folders, but cannot be deleted nor files can be added to these folders.
IEC61850: IEC 61850 configuration (CID) file can be added to this folder to activate the IEC 61850 protocol functions of the meter.
optionModuleUpg and rmdUpg: Firmware update files can be loaded for the meter’s remote display or option modules into these folders.
documents: this folder is intended for user storage. Any type of files can be read, written, deleted in this folder.
web: This folder is where the meter’s default webpages are stored and where custom webpages can be added to the meter by copying them into the appropriate subfolders.

Schneider Electric Egypt and North East Africa