Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the difference between Conventional enclosed thermal current (Ithe) and Conventional free air thermal current (Ith)?
Conventional enclosed thermal current (Ithe):
The conventional enclosed thermal current is the value of current stated by the manufacturer to be used for the temperature-rise tests of the equipment when mounted in a specified enclosure. The value of the conventional enclosed thermal current shall be at least equal to the maximum value of the rated operational current of the enclosed equipment in eight-hour duty. If the equipment is normally intended for use in unspecified enclosures, the test is not mandatory if the test for conventional free air thermal current (Ith) has been made. In this case, the manufacturer shall be prepared to give guidance on the value of enclosed thermal current or the derating factor.

Conventional free air thermal current (Ith):
The conventional free air thermal current is the maximum value of test current to be used for temperature-rise tests of unenclosed equipment in free air. The value of the conventional free air thermal current shall be at least equal to the maximum value of the rated operational current of the unenclosed equipment in eight-hour duty. Free air is understood to be air under normal indoor conditions reasonably free from draughts and external radiation.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: