{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are the equivalent software modules when upgrading PME HC or DC Edition to PME 9.0 or newer?

Issue
PME 9.0 was not released with separate Healthcare (HC) and Data Center (DC) editions, so there may be a need to understand what equivalent software modules are available that would effectively replace the additional functionality that came with the HC and DC editions of PME 7.2.2 and PME 8.2.

Product Line
Power Monitoring Expert 7.2.2  (Base, Healthcare, and Data Center)
Power Monitoring Expert 8.2  (Base, Healthcare, and Data Center)
Power Monitoring Expert 9.0/2020

Environment
Software Upgrade
Licensing

Resolution

PME 7.2.2 or PME 8.2 HC Edition
  • UpgradingPME 7.2.2 or PME 8.2 HC edition base licenses will yield activation IDs for the modules mentioned below when upgraded via software assurance included in a digital service plan
  • The following modules are the PME 9.0/2020 version equivalent to PME 7.2.2 or PME 8.2 HC Edition
    • PME 9.0 Base/PME 2020 Base
    • Backup Power Module
    • Insulation Monitoring Module
PME 7.2.2 or PME 8.2 DC Edition
  • The DC edition is very similar to the base edition except it includes pre-configured Vista diagrams, graphics, VIP frameworks, logical device scripts, etc.
  • Therefore, the PME 9.0/2020 version equivalent to PME 7.2.2 or PME 8.2 DC Edition is just the base edition:
    • PME 9.0 Base/PME 2020 Base
For more information on PME 9.0 software modules, refer to the Software Modules section of the PME 9.0 System Guide.
For more information on PME 2020 software modules, refer to the Software Modules section of the PME 2020 System Guide.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: