Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Is the CANopen Communication DTM available and operational for the BMECXM0100 module on M580 platform?
1. Issue

The customer wants to know if the CANopen Communication DTM is available and operational for the BMECXM0100 module on M580 platform.
2. Product Line

BMECXM0100
Unity Pro / EcoStruxure Control Expert
3. Environment

CANopen CommunicationDTM version 1.1.2 (identified on this version, also valid for previous and next versions)
4. Resolution

No, the CANopen Communication DTM is not designed to operate with M580 and with BMECXM0100, but the CXM Master Gateway DTM helps configuring the BMECXM0100 and provides a first level of configuration and diagnostic of the devices.

To configure, adjust, control and monitor the drives and motor control devices, use SoMove software.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: