{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Will the display still be active if a ModBus network is attached to the ATS22?

Article available in these languages: Czech

Issue:
Wanting to control, the ATS22, with the Modbus network and also be able to use the remote keypad display.

Product Line:
Altistart 22

Environment:
All models and serial numbers

Cause:
N/A

Resolution:
The ATS22 soft starter has a built in display, as part of the soft starter. The RJ-45 port can be used for a remote mounted display keypad or for Modbus network. If the RJ-45 port is used for communications or for remote keypad the local display on the soft starter control board will still operate. The port can not be used for both a remote keypad and for Modbus communication.

Schneider Electric Egypt and North East Africa