Search FAQs
How do I configure a NOC301/311 for no gateway when the DTM will not accept a gateway address of 0.0.0.0.
Issue
How do I configure a BMENOC0301 or BMENOC0311 for 'no gateway' when the DTM will not accept a gateway address of 0.0.0.0?
Product Line
BMENOC0301
BMENOC0311
Environment
Unity, Control Expert
Resolution
The user can enter the BMENOC IP address as the gateway IP which will essentially direct any gateway traffic to itself which will would be as if he had no gateway configured. This is a common practice to avoid entering 0.0.0.0 as a configured gateway address.
How do I configure a BMENOC0301 or BMENOC0311 for 'no gateway' when the DTM will not accept a gateway address of 0.0.0.0?
Product Line
BMENOC0301
BMENOC0311
Environment
Unity, Control Expert
Resolution
The user can enter the BMENOC IP address as the gateway IP which will essentially direct any gateway traffic to itself which will would be as if he had no gateway configured. This is a common practice to avoid entering 0.0.0.0 as a configured gateway address.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: