{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a NetBotz Door Switch Sensor be installed onto NetShelter SX with RACS?
Issue:
There are no holes in the Rack Air Containment frame (front or rear) for the NetBotz Door Switch Sensor install onto.

Product Line:
NetBotz NBES0301, NBES0302
HACS ACCS1006, ACCS1007

Environment:
All versions and serial ranges.

Cause:
The frame of the Rack Air Containment does not include the pre-drilled holes for NetBotz that the NetShelter SX does.

Resolution:

The NetBotz Door Switch Sensors can be installed using the included 2-sided tape. Please see the attached document.

Schneider Electric Egypt and North East Africa

Attachment(s)
20191015 Mounting NetBotz Door Switch Sensors onto NetShelter SX with RACS.pdf [1.26 MB]