{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a 3rd party UPS be installed in the AR106V or AR106VI?
Issue:
It is unknown if a 3rd Party UPS can be installed into the AR106V and AR106VI.


Product Line:
AR106V, AR106VI

Environment:
All versions and serial ranges.

Cause:
The NetShelter WX 6U Vertical cabinets have a mounting bracket for a 2U UPS.

Resolution:

Any 3rd party UPS must be validated by the manufacturer to work with this cabinet prior to installation:
The manufacturer must validate that the 3rd party UPS can be installed vertically. Not all batteries can install in this orientation.
When shipping with a 3rd party UPS installed, the manufacturer must validate that the 3rd party UPS can ship installed using their rail kit(s), without disconnecting in transit.

Schneider Electric Egypt and North East Africa