This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Configuring the local date and time allows using time-based features such as activating day/night welcome scenes, Night Light button and Sleep mode for Glass Touch Panel. The HRC supports Time synchronization from a BACnet network. Make sure to click SAVE before navigating to a different section. HRC reboot is required to apply the changes