This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
- Run the Device Administrator and select the AS/AS-P/AS-B to be upgraded and select the upgrade button, you will be presented with this menu.
- Select Apply hotfix and you will be presented with the window as shown below.
- Select the OK button and you will be presented with a window to select the hotfix file.
Locate the hotfix file, i.e. SmartX.Server-3.0.3.11-Hotfix.exe. When the Open button is selected the SmartX server upgrade will begin immediately.
Warning: if the file fails to load please check the PC has access to the internet as this is required to validate the integrity of the file.
Note, the hotfix file is a self-extracting archive and will be extracted to the DA folder by DA. - When complete, logon to workstation and verify the running build is correct.