{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Adding a ATV900 series VFD to the NOC DTM Browser
Title
Setup of a ATV900 series VFD in the NOC DTM Browser

Issue
Show how to add a ATV900 series VFD to the NOC DTM browser

Product Line
M580 BMENOC03x1

Environment
Unity Pro DTM Browser

Resolution
To compliment a video that adds a ATV900 series VFD to the NOC DTM browser, below is the step by step procedure.
First, in the DTM Browser select the BMENOC0321 and from the Right Click Mouse menu select Add in the menu.
Select the ATV9xx device and click Add DTM button.
Select the Modbus protocol.
Enter the name for your DDT variable.
Double Click your DDT variable entry and select Standard Drive Wall Mounting
Then select the appropriate ATV900 series part number from list. For example select the ATV930U75M3 VFD part number

After the SoMove DTM opens Select the Parameter List Tab, expand the Port - Modbus TCP/EthernetIP entry
Select Generic Setting and note that IP address that the settings for the IP address are grayed out
To Change IP address parameters assigned to VFD, Double click on the BMENOC0321 in DTM Browser
In the BMENOC0321 configuration window, Scroll down to Device List and Select the Device [007] ATV9_MBT1.
Then Select Address Setting Tab and enter the IP address to use for the ATV900 VFD
Note that the IP address was updated to new value in the SoMove DTM

Now, Select Protocol & Drive Profile entry and note that the Protocol Modbus TCP is already selected but it is grayed out and can not be changed.
Next, there are three IO Profiles to chose from so select the Default Profile
Next, Scroll down to setup the ModbusTCP Input/Output Tables
Right click line 3 and select Add to add a new parameter to the Input table
For example, select CRC and CCC from Table to add them

Next, Scroll to right for Outputs Table Window and right click line 3 and select Add
For Example, select OL1R from Table to add it to the Output table
Select OK to set changes to Inputs and Outputs Table

Finally, Double click on the BMENOC0321 in DTM Browser and in the BMENOC0321 configuration window scroll down to the Device List
Select the Device [007] ATV9_MBT1 and then select Request Setting Tab.
Note that the Read and Write requests are already setup and the DDT tags variables are complete

Schneider Electric Egypt and North East Africa