Search FAQs
Vijeo Designer 6.2 cannot launch after updating to Windows 10 build 1903
Issue:
After upgrading to Windows 10 Build 1903, Vijeo Designer V6.2 no longer launches and gives error code (0xc0150002).
Product Line:
Vijeo Designer (all versions)
Resolution:
Upon updating to Windows 10 Build 1903, Vijeo Designer 6.2 may fail to launch. The new update provided by Microsoft somehow disturbs the Microsoft Visual Studio 2005 SP1 C++ Redistributable libraries required by Vijeo Designer. The solution is to re-install the Microsoft Visual Studio 2005 SP1 C++ Redistributable libraries using the attached file installation package.
NOTE: Windows 10 build 1903 may also block running any file that did not originate from the Microsoft App Store. To workaround this, you will need to goto Settings->Apps->Apps & Features and change the setting for "Choose where to get apps" from "The Microsoft Store only (recommended)" to " Anywhere".
![Apps menu Apps menu](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009DZC9QAO&oid=00DA0000000abSm)
Please find the needed file attached to this FAQ document.
After upgrading to Windows 10 Build 1903, Vijeo Designer V6.2 no longer launches and gives error code (0xc0150002).
Product Line:
Vijeo Designer (all versions)
Resolution:
Upon updating to Windows 10 Build 1903, Vijeo Designer 6.2 may fail to launch. The new update provided by Microsoft somehow disturbs the Microsoft Visual Studio 2005 SP1 C++ Redistributable libraries required by Vijeo Designer. The solution is to re-install the Microsoft Visual Studio 2005 SP1 C++ Redistributable libraries using the attached file installation package.
NOTE: Windows 10 build 1903 may also block running any file that did not originate from the Microsoft App Store. To workaround this, you will need to goto Settings->Apps->Apps & Features and change the setting for "Choose where to get apps" from "The Microsoft Store only (recommended)" to " Anywhere".
Please find the needed file attached to this FAQ document.
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Range:
Explore more
Range: