{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can the HMIGTUx be used with a normal HMIDT screen?

Article available in these languages: Spanish

Issue:
There is no information regarding if the HMIGTUx series is compatible with the HMIDT series screens and vice versa.

Product Line:
HMIGTUx, HMIGTU, HMIG3X, HMIG3U, HMIG5U, HMIG5U2

Resolution:
When using the HMIGTUx series (HMIG3X), it must be paired with an HMIDT35X, HMIDT65X, or a HMIDT75X. It is not possible to use HMIDT (non-extreme) with an HMIG3X. Vijeo Designer is not able to recognize this combination.

Similarily, it is not possible to use the HMIG3U, HMIG5U, HMIG5U2 with the HMIDTx (extreme) displays.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: