{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can we access the fieldbus network of BMENOC0321 via its front ports?
  1. Issue
When ip forwarding service is activated, the BMENOC0321 makes its fieldbus network configurable and automatically enables its backplane port.
Then can we access(ping) the fieldbus network of BMENOC0321 via its front ports?
  1. Environment
N/A
  1. Resolution
No, the fieldbus network address is not accessible via BMENOC0321’s front ports.
It is only accessible via M580 or other Ethernet module(for ins. BMENOC0301) when the other module’s backplane port is enabled.

Schneider Electric Egypt and North East Africa