{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it supported to add sound file for alarm in VXD/EOTE
  1. Issue
Is it supported to add sound file like mp3/wav for alarm in Vijeo XD / EcoStruxure Operator Terminal Expert .
  1. Environment
Vijeo XD / EcoStruxure Operator Terminal Expert V3.1.
  1. Resolution
No, user can’t add/import specified external sound file into EOTE for alarm, but can use the beep operation in project, the panel will start to beep when the trigger occurs.

Schneider Electric Egypt and North East Africa