{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

Is the Vertical Installation Supported for EcoStruxure Building Operation SmartX Controller (MP-C)?

The MP-C is typically installed horizontally (on a DIN rail going from left to right), with the device label text in the upright position reading left to right.

The MP-C can also be installed vertically (on a DIN rail going from top to bottom), which means that the device is rotated +90 degrees or -90 degrees from the horizontal position. Installing the MP-C face down from a ceiling or face up on a horizontal surface is not supported.
Machine generated alternative text:Figure: Restrictions regarding the installation orientation

Rooftop Applications:
Install the MP-C horizontally in rooftop applications, -40 to +60 °C (-40 to +140 °F), to ensure that the device stays within the thermal specifications. Failure to follow these instructions can result in equipment damage.
Machine generated alternative text:mulli7.—s111F.i. . L.


Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: