{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a logic input be assigned to the external fault in ATV320 drive?

Article available in these languages: Spanish

Issue:
How can I configure an external fault using logic input in ATV320 drive?

Product Line:
ATV320 drive

Environment:
All Serial numbers

Cause:
Application requires an external fault via a logic input.

Resolution:
Yes, a logic input can be assigned to a external fault.
External Fault can be accessed:  DRI- > CONF > FULL > FLT- > EtF- > EtF
Then assign (LI1) to (LI6), logic input that is not assigned to any other functions.

Logic can be configured (LEt) As LO [Active low] (LO) or HIG [Active high] (HIG)(default).
It defines the positive or negative logic of the input assigned to the detected fault.
Configure EPL [External fault mgt]  for Type of stop in the event of an external fault.

Schneider Electric Egypt and North East Africa