This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
The Altistart 48 connected in the motor supply line
The motor connection depends on the supply voltage, which in this example is a star connection.

The motor connection depends on the supply voltage, which in this example is a delta connection.

The Altistart 48 connected in the motor delta winding
ATS48***Q or ATS48***YS316 starters connected to motors with delta connections can be inserted in series in the motor windings. They are powered by a current which is less than the line current by a factor of SQRT 3, which enables a starter with a lower rating to be used.

The motor connection depends on the supply voltage, which in this example is a star connection.
The motor connection depends on the supply voltage, which in this example is a delta connection.
The Altistart 48 connected in the motor delta winding
ATS48***Q or ATS48***YS316 starters connected to motors with delta connections can be inserted in series in the motor windings. They are powered by a current which is less than the line current by a factor of SQRT 3, which enables a starter with a lower rating to be used.
Released for: Schneider Electric Egypt and North East Africa