When importing the CanOpen EDS file “IS620P_CO_V056” with Hardware Catalog Manager, an error occurs shown as below snapshot.
The workaround for now is to set the Datatype=0x0006 [unsigned16] (previous value is 0x0005 [unsigned8]) in object [2011sub3F] and then you can import the CanOpen EDS without error.
- Product Line
- Environment
The workaround for now is to set the Datatype=0x0006 [unsigned16] (previous value is 0x0005 [unsigned8]) in object [2011sub3F] and then you can import the CanOpen EDS without error.
Released for:Schneider Electric Egypt and North East Africa