SmartX IP Controller – RP-C is a room-purpose, fully programmable, IP based field controller that suits a wide range of HVAC applications. The freely programmable RP-C models provide flexibility through support of both Script and Function Block programming options.
Save time and increase the repeatability in a project with pre-designed standard room applications for fan coil and chilled beam systems. Each standard application comes with graphics, functional description, I/O wiring diagram, sequence of operations and a set of other documents. The applications can be downloaded from The Exchange Building & Power Extranet and used together with Building Operation WorkStation or directly from the SmartX e-Commission tool.
1. Open a web browser and navigate to https://bms-applications.schneider-electric.com/
2. In ‘BMS Applications’, filter on the type of RP-C model and type of application to
use.
3. Select the preferred application and download the image file to your Android
tablet.
4. Download the custom type file to your computer.
Released for: Schneider Electric Egypt and North East Africa