Issue
If you try to change the slot configuratiopn for a Profibus ifm10DBB slave device in the 'Prosoft Configurator for Modicon' software, the drop down list box could be blank.
Product Line
PMEPXM0100
Environment
Windows 10
Resolution
If you try to change the slot configuratiopn for a Profibus ifm10DBB slave device in the 'Prosoft Configurator for Modicon' software, the drop down list box could be blank.
The cause of the issue is due to the software failing to decode the gsd file when the allowable slot module range (“x-y”) starts with zero. (i.e. x = 0).
Note: There is no issue when the allowable modules are in a list e.g. 0,1,2,3,4… or if the module range does not start with zero, e.g. 1-5 or 100-115
To resolve the issue,
Change the “Allowable Module Range from 0-4, to 0,1-4.
If you try to change the slot configuratiopn for a Profibus ifm10DBB slave device in the 'Prosoft Configurator for Modicon' software, the drop down list box could be blank.
Product Line
PMEPXM0100
Environment
Windows 10
Resolution
If you try to change the slot configuratiopn for a Profibus ifm10DBB slave device in the 'Prosoft Configurator for Modicon' software, the drop down list box could be blank.
The cause of the issue is due to the software failing to decode the gsd file when the allowable slot module range (“x-y”) starts with zero. (i.e. x = 0).
Note: There is no issue when the allowable modules are in a list e.g. 0,1,2,3,4… or if the module range does not start with zero, e.g. 1-5 or 100-115
To resolve the issue,
- Open the .gsd file with Wordpad
- Locate the Slot(x) line for the slot that is having the problem.
- Change the “Allowable Module Range from 0-4, to 0,1-4. (See example below).
- Save the changes.
- Retest.
Change the “Allowable Module Range from 0-4, to 0,1-4.
From:
Slot(1) = "Slot 1: DI/DO S/A-Slaves AS-i 1" 1 0-4
To:
Slot(1) = "Slot 1: DI/DO S/A-Slaves AS-i 1" 1 0,1-4
Slot(1) = "Slot 1: DI/DO S/A-Slaves AS-i 1" 1 0-4
To:
Slot(1) = "Slot 1: DI/DO S/A-Slaves AS-i 1" 1 0,1-4
Released for:Schneider Electric Egypt and North East Africa