Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
What kind of microphone can I use on a NetBotz appliance / Camera pod 160?
Issue:
What kind of microphone can I use on a NetBotz appliance / Camera pod 160?

Product Line:
NetBotz

Environment:
NetBotz version 3 appliances (NBRK0355, NBRK0455, NBPD0160)

Cause:
NetBotz appliances and / or Camera pods are capable of using external microphones.

Resolution:
The proper microphone to connect to a NetBotz is a stereo dynamic (non condenser) microphone with a 3.5 mm jack. It is advised that you do not use a directional or "shotgun" microphone.
 

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: