Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
How is OPR output power calculated on an ATV320 drive?
Issue
How does ATV320 calculate OPR output power ?

Product Line:
Altivar 320

Environment:
All model numbers, all serial numbers

Cause:
N/A

Resolution: 
To calculate the value for OPR (motor power), the ATV320 uses this formula:
Voltage * Current * Sqrt(3) * Power factor.
Voltage and current can be viewed in the VFD  monitoring menu.
The OPR value is based on the rated motor power programmed in the unit and has a range of 0 to 2.5 X the rated motor power (NPR) value.  This means 100% equals rated motor power (NPR).
 

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: