{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PM5500 “invalid parameter” error in ION Setup
Issue
There is an error showing “Invalid Parameter” when changing PM5500 Basic Setup parameters in ION Setup

Product Line
PM5500 series
ION Setup

Environment
Meter setup & commissioning

Issue
A bug was found in ION Setup v3.2.19323.01 where most parameters could not be changed for the PM5500 meter series.

Resolution
Option1
Downgrade to ION Setup v3.1.19.19276.0.1 or older attached.

Option2
Issues are resolved in ION Setup v3.2.19350.01 set to be released late Jan 2020.

For latest ION Setup download see FA212816.

Schneider Electric Egypt and North East Africa