{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Easergy P5 P5x30 and P5x20: Is there a flush mounting accessory for the relay?

Easergy P5 can be installed with or without a flush mounting accessory. Using the flush mounting accessory helps to reduce the installation time thanks to the automatic fixing system and to achieve IP51 from the the front.

The following references are available:
REL51032: 20TE
REL51052: 30TE

Schneider Electric Egypt and North East Africa