{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Breaking down HP rating of an Enclosed ATS22 soft start.
Issue:
How do I identify the horsepower when reading the catalog number for an ATS22 863922U ?

Product Line:
8639  8638

Environment:
22F, 22T,  22U

Cause:
Catalog Number identification


Resolution:
The letter following the Class and Type represents the horsepower,
Catalog Number Example: 863922UDG4BA06A07
863922U (D) G4BA06A07 (D) = 10hp horsepower

A = 3 hp
B = 5 hp
C = 7.5 hp
D = 10 hp
E = 15 hp
F = 20 hp
G = 25 hp
H = 30 hp
J = 40 hp
K = 50 hp
L = 60 hp
M = 75 hp
N = 100 hp
P = 125 hp
Q = 150 hp
R = 200 hp
S = 250 hp
T = 300 hp
U = 350 hp
X = 500 hp

Schneider Electric Egypt and North East Africa